S32KXX Development Package Could Not Be Installed for S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32KXX Development Package Could Not Be Installed for S32DS

2,744 Views
utkuf
Contributor I

When I try to install S32K3XX Development Package from S32DS Extensions and Updates window in S32DS.3.5, unfortunately it could not be installed, there is an error. How could I solve this issue?

0 Kudos
Reply
3 Replies

2,636 Views
utkuf
Contributor I

I have installed successfully, however right now, I got an error like "Description Resource Path Location Type
fatal error: OsIf_Cfg.h: No such file or directory Can_Example_S32K344 line 45, external location: C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\BaseNXP_TS_T40D34M30I0R0\include\OsIf_Internal.h C/C++ Problem"

0 Kudos
Reply

2,616 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @utkuf 

Before running the example, a configuration needs to be generated. First, go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu, then click on the desired configuration tool (Pins, Cocks, Peripherals etc...). Clicking on any one of those will generate all the components. Make the desired changes (if any), then click on the "S32 Configuration Tool->Update Code" button.

0 Kudos
Reply

2,723 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @utkuf 

There is an S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices. Did you already have it?

Take a look at this community post. Here is mentioned information about it.

Please let me know if you still have problems.

 

B.R.

VaneB

0 Kudos
Reply