S32K3xx development package installation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx development package installation problem

4,354 Views
AbdullahRz
Contributor I

Hello,

I'm trying to install the S32K3xx development package but getting the following error:

Operation detailsSoftware being installed: com.nxp.s32ds.platform.ide.feature.feature.group 3.4.3.202112151555 Missing requirement: com.freescale.s32ds.cross.sdk.support 1.0.0.202112151547 requires 'osgi.bundle; org.eclipse.jgit 0.0.0' but it could not be found Cannot satisfy dependency: com.nxp.s32ds.cle.arm.mbs.arm64.linux.gnu.10.2 1.0.0.202112151550 depends on: osgi.bundle; com.freescale.s32ds.cross.sdk.support 0.0.0 Cannot satisfy dependency: com.nxp.s32ds.cle.arm.mbs.arm64.linux.gnu.10.2.feature.feature.group 1.0.0.202112151550 depends on: org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.arm.mbs.arm64.linux.gnu.10.2 [1.0.0.202112151550,1.0.0.202112151550] Cannot satisfy dependency: com.nxp.s32ds.platform.ide.feature.feature.group 3.4.3.202112151555 depends on: org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.arm.mbs.arm64.linux.gnu.10.2.feature.feature.group [1.0.0.202112151550,1.0.0.202112151550]

I tried the method explained in this link: https://community.nxp.com/t5/S32-Design-Studio/S32K3xx-development-package-could-not-be-installed/td...

but still getting the same error : 

Cannot complete the install because one or more required items could not be found.
Software being installed: S32K3xx development package 1.0.0.202112162057 (com.nxp.s32ds.s32k3.dev.feature.feature.group 1.0.0.202112162057)
Missing requirement: S32 Design Studio SDK support 1.0.0.202112151547 (com.freescale.s32ds.cross.sdk.support 1.0.0.202112151547) requires 'osgi.bundle; org.eclipse.jgit 0.0.0' but it could not be found
Cannot satisfy dependency:
From: S32 Design Studio Bundle for Supporting Migration 1.0.0.202112151547 (com.nxp.s32ds.cle.cdt.migration 1.0.0.202112151547)
To: osgi.bundle; com.freescale.s32ds.cross.sdk.support 0.0.0
Cannot satisfy dependency:
From: S32 Design Studio CLE S32K3 DEV 1.0.0.202112162053 (com.nxp.s32ds.cle.s32k3.s32k3.dev.feature.feature.group 1.0.0.202112162053)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.s32k3.s32k3.dev.migration [1.0.0.202112162053,1.0.0.202112162053]
Cannot satisfy dependency:
From: S32 Design Studio CLE S32K3xx Migration 1.0.0.202112162053 (com.nxp.s32ds.cle.s32k3.s32k3.dev.migration 1.0.0.202112162053)
To: osgi.bundle; com.nxp.s32ds.cle.cdt.migration 0.0.0
Cannot satisfy dependency:
From: S32K3xx development package 1.0.0.202112162057 (com.nxp.s32ds.s32k3.dev.feature.feature.group 1.0.0.202112162057)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.s32k3.s32k3.dev.feature.feature.group [1.0.0.202112162053,1.0.0.202112162053]

0 Kudos
Reply
1 Reply

4,319 Views
mikedoidge
NXP Employee
NXP Employee

Hello @AbdullahRz,

Apologies for the long delay in reply.

Can you retry after deleting S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.core\cache\ and S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.repository\cache\?

Best Regards,

Mike