Hello.
I try import S32K312 example projects into S32DS v3.5.
S32K312 Example Link:
https://community.nxp.com/t5/S32K-Knowledge-Base/All-Example-S32K312-DS3-5-RTD-3-0-0/ta-p/1790004
I have below error message.
Here is my S32DS information:
How can I get S32K312 example projects that working with S32DS v3.5 ?
Best Regards,
Sean Sung.
解決済! 解決策の投稿を見る。
Hi
I checkd the files in S32K312_I2C_LPI2C_DMA_working\RTD\src. This project was based on S32K3_RTD_3_0_0_P01_HF02_D2305.
So please install S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
I checkd the files in S32K312_I2C_LPI2C_DMA_working\RTD\src. This project was based on S32K3_RTD_3_0_0_P01_HF02_D2305.
So please install S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello @Robin_Shen
I can load project after install RTD HF02.
Thank you for support.
Best Regards,
Sean Sung.