S32K312 example import error in S32DS v3.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K312 example import error in S32DS v3.5

跳至解决方案
977 次查看
ssean
Contributor IV

Hello.

I try import S32K312 example projects into S32DS v3.5.

S32K312 Example Link:

https://community.nxp.com/t5/S32K-Knowledge-Base/All-Example-S32K312-DS3-5-RTD-3-0-0/ta-p/1790004

I have below error message.

ssean_0-1729135317378.png

ssean_1-1729135324731.png

 

Here is my S32DS information:

ssean_2-1729135357538.png

ssean_3-1729135364448.png

 

How can I get S32K312 example projects that working with S32DS v3.5 ?

 

Best Regards,

Sean Sung.

标记 (1)
0 项奖励
回复
1 解答
951 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I checkd the files in S32K312_I2C_LPI2C_DMA_working\RTD\src. This project was based on S32K3_RTD_3_0_0_P01_HF02_D2305.

So please install S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
952 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I checkd the files in S32K312_I2C_LPI2C_DMA_working\RTD\src. This project was based on S32K3_RTD_3_0_0_P01_HF02_D2305.

So please install S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
917 次查看
ssean
Contributor IV

Hello @Robin_Shen 

I can load project after install RTD HF02.

Thank you for support.

 

Best Regards,

Sean Sung.

标记 (1)
0 项奖励
回复