S32K144:SPI Transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144:SPI Transfer

4,736件の閲覧回数
bjrajendra
Senior Contributor I

Hello all,

I tried to use SPI transfer with CS as GPIO. I'm performing following steps.

1. Making the CS LOW

2. Pushing to data in the FIFO

3. Making the CS HIGH

I'm able to transfer the data but my CS goit HIGH (Step 3) Far ahead of the transfer.

CS_LOW;

LPSPI0->TDR = LPSPI_TDR_DATA(n) ; 
while((LPSPI0->SR & LPSPI_SR_TDF_MASK)>>LPSPI_SR_TDF_SHIFT==0) {} 

CS_HIGH;

Kindly help in this regard,

Raju

ラベル(1)
タグ(3)
0 件の賞賛
返信
5 返答(返信)

4,468件の閲覧回数
wjandsq
Contributor IV

/* SPI FLASH Sequence for 1 bytes is OK */

LPSPI1->TCR = ((LPSPI1->TCR) | (LPSPI_TCR_BYSW_MASK));
LPSPI1->TCR = ((LPSPI1->TCR) & (~LPSPI_TCR_BYSW_MASK));
LPSPI1->FCR = 0x00000003; /* RXWATER=0 TXWATER=3 */
lpspi_tmp = ((LPSPI1->TCR) & (~LPSPI_TCR_FRAMESZ_MASK));
LPSPI1->TCR = (lpspi_tmp | (7U & LPSPI_TCR_FRAMESZ_MASK));

PINS_DRV_ClearPins(PTB, 1 << 17); /* Software Control PCS3 : SET PCS3 LOW */

while (((LPSPI1->SR & LPSPI_SR_TDF_MASK) >> LPSPI_SR_TDF_SHIFT) == 0);
LPSPI1->TDR = ( uint32_t ) (*txdata_p++);  /* for 1 bytes */
LPSPI1->TCR = ((LPSPI1->TCR) | (LPSPI_TCR_TXMSK_MASK)); /* Start Transmit and Hardware Auto Clear */
LPSPI1->TCR = ((LPSPI1->TCR) & (~LPSPI_TCR_RXMSK_MASK));
LPSPI1->SR |= LPSPI_SR_TDF_MASK; /* Clear TDF flag */
while (((LPSPI1->SR & LPSPI_SR_RDF_MASK) >> LPSPI_SR_RDF_SHIFT) == 0);
lpspi_tmp = LPSPI1->RDR;
*rxdata_p++ = ( uint8_t ) (lpspi_tmp >> 0);
while (((LPSPI1->SR & LPSPI_SR_FCF_MASK) >> LPSPI_SR_FCF_SHIFT) == 0);

LPSPI1->SR  |= LPSPI_SR_RDF_MASK | LPSPI_SR_FCF_MASK;
LPSPI1->TCR = ((LPSPI1->TCR) & (~LPSPI_TCR_CONTC_MASK));
LPSPI1->CR = 0x00000000; /* Module Disable、Debug Disable */
PINS_DRV_SetPins(PTB, 1 << 17); /* Software Control PCS3 : SET PCS3 High */

0 件の賞賛
返信

4,468件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

here's the difference:

pastedImage_1.png

pastedImage_2.png

That means you need to wait for TCF flag, not for TDF.

Regards,

Lukas

0 件の賞賛
返信

4,468件の閲覧回数
bjrajendra
Senior Contributor I

Hi Lukas,

Thanks for the response.

I tried waitng till 

while((LPSPI0->SR & LPSPI_SR_TCF_MASK)>>LPSPI_SR_TCF_SHIFT==0) {} 

Even I tried to wait for the FCF flag to set. I don't see any change considering by frame length as 7+1 bits

 

pastedImage_1.png

 

but, stranges the TCF, FCF, WCF flag will set immeadiately after writing the data into the tranmit buffer though theCS still holds the LOW.

 

Kindly help in this regard,

Raju

0 件の賞賛
返信

4,468件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

That's a good point, I did quick test and I can see that too. TCF flag is obviously set when data are transferred to shift register and physical transmission is not considered.

But in fact, the description is correct:

"In master mode when the LPSPI returns to idle state with the transmit FIFO empty, the Transfer Complete Flag will set."

In other words, TCF is set immediately when FIFO is empty.

As a workaround, you can use delay loop instead for waiting for flag. Just calculate required time for your SPI frequency.

Regards,

Lukas

0 件の賞賛
返信

4,468件の閲覧回数
bjrajendra
Senior Contributor I

Thanks Lukas for the Support.

In fact, using a delay loop is not a good idea I feel. Any other idea is greatly appreciated.

Raju