S32K1 RTM Lin Stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1 RTM Lin Stack

5,526 Views
ke
Contributor I
hello,
 
I'm trying to move our projects from S32 SDK to RTD. S32K116/144/148 are used in our projects.
I installed the following software:
S32DS 3.5
S32K1xx development package 3.5.0
S32K1 RTD AUTOSAR 4.4 Version 1.0.1 HotFix 01
 
And tried to install the lin stack with S32K1_LINSTACK_RTM_1_0_2_CD01_D2209.zip but failed:
Screenshot 2023-07-13 113541.pngScreenshot 2023-07-13 113611.png
 
From this thread it seems the lin stack 1.0.1 is needed.
The problem is, I cannot find the lin stack version 1.0.1
Screenshot 2023-07-13 124146.png
Please someone from NXP could let me know how to fix this issue. Thanks!

 

0 Kudos
Reply
9 Replies

5,481 Views
ke
Contributor I

Hi @VaneB 

thanks for the answer. Could you please tell me where can I find the "Real Time Drivers (RTD) SW32M244 RTD 4.4 1.9.0 CD01 package"?

I searched in s32ds extensions and updates, also the "Software & Support" "Product List" in nxp website, but cannot find it.

 

0 Kudos
Reply

5,463 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ke 

This package is still a code drop, so you need to request access, for this, please contact your NXP representative for further support in this part. 

Another option is to use the previous version of the Lin stack. 

0 Kudos
Reply

5,368 Views
ke
Contributor I

Hi @VaneB 

Could you tell me where can I get the previous version (1.0.1) of the Lin Stack? Thanks!

0 Kudos
Reply

5,345 Views
VaneB
NXP TechSupport
NXP TechSupport

@ke 

You can download it from our website at S32K1 Reference Software -> Automotive SW - S32K1 - LIN Stacks -> Previous tab.

VaneB_0-1689870510667.png

0 Kudos
Reply

5,262 Views
ke
Contributor I

Hi @VaneB 

the Previous tab is not available.

Screenshot 2023-07-25 085032.png

0 Kudos
Reply

5,244 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ke 

The reason for this is that when you enter Automotive SW - S32K1 Reference Software -> Automotive SW - S32K1 - LIN Stacks, you click the SW32K1 LIN stack version 1.0.2 CD01. Once there, you do not see the previous tab. What you need to do is not click SW32K1 LIN stack version 1.0.2 CD01.

Please refer following image. 

VaneB_0-1690315236361.png

 

0 Kudos
Reply

5,500 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ke 

In the release notes it is mentioned that you must have installed the Real Time Drivers (RTD) SW32M244 RTD 4.4 1.9.0 CD01 package.

Also, according to the error you shared, it is also mentioned that you need to install this package.

 

B.R

VaneB

0 Kudos
Reply

4,714 Views
danyal
Contributor I

Hello @VaneB

I am facing the same issue, it worked for me in the past year when i had version 3.4 of Design Studio and LIN STACK RTM 1.0.1 and RTD 101 Package

But now i have Design Studio 3.5 with RTD 4.4 R21-11 2.0.0, this is the only RTD available. I am trying to get LIN STACK RTM 1.0.2 which fails like @Vojtech and Is asking for "Real Time Drivers (RTD) SW32M244 RTD 4.4 1.9.0 CD01 package". where can i download that? since the only one available is 2.0.0. 
Thanks 

0 Kudos
Reply

4,959 Views
Vojtech
Contributor II

Hello VaneB,

we are still facing the issue described in this post: Possible bug in LIN stack..? - NXP Community

The issue was corrected in LIN stack v1.0.2 CD01 (so usage of LIN stack v1.0.1 does not help )

LIN stack v1.0.2 CD01 installation fails as well to me:

Vojtech_0-1694590471822.png

 

I was trying to find "Real Time Drivers (RTD) SW32M244 RTD 4.4 1.9.0 CD01 package" but I could not find it even today. Is it still "hidden"?

Do we really need this SW32M244 RTD even for mcu S32K148 ?

How should we proceed?

Thank you

Vojtech