S32K Design Studio Install Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Design Studio Install Error

1,369 Views
fadsfasdf
Contributor I

when I Install Design Studio, The following error is appeared.

And I couldn't open the program. 

!SESSION 2022-08-21 13:37:14.180 -----------------------------------------------
eclipse.buildId=unknown
java.version=1.8.0_202
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=ko_KR
Command-line arguments: -os win32 -ws win32 -arch x86_64

!ENTRY org.eclipse.osgi 4 0 2022-08-21 13:37:15.096
!MESSAGE Application error
!STACK 1
java.lang.IllegalStateException: Unable to acquire application service. Ensure that the org.eclipse.core.runtime bundle is resolved and started (see config.ini).
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:81)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:657)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:594)
at org.eclipse.equinox.launcher.Main.run(Main.java:1465)

 

How can I solve that Provlem 

0 Kudos
Reply
1 Reply

1,353 Views
mikedoidge
NXP Employee
NXP Employee

Hello @fadsfasdf,

Would you please provide the installation log file?

It can be located in a folder like: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs

Best Regards,
Mike

0 Kudos
Reply