S32K Debug Stuck at 99%

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Debug Stuck at 99%

3,701 Views
bjrajendra
Senior Contributor I

Hello all,

Currently, I'm using the S32K146 device ith S32DS IDE,

I tried to program & debug the software but it got stuck at 99%. Failed to program the software.

 pastedImage_1.png

Unfortunately, it didn’t download and got stuck at 99% even after a long time.

Kindly suggest if I missed something

Raju

Tags (1)
0 Kudos
Reply
2 Replies

2,798 Views
juan_see
Contributor III

Hi all, 

 

The plugin you are using it is a bit outdated. PEmicro's latest official plugin is 5.3.6.202210191804. To update the plugin, please follow the steps outlined in the following blogpost:

 

https://www.pemicro.com/blog/index.cfm?post_id=124

 

You do not need to install the "PEmicro ARM Device Expansion Plugin"

0 Kudos
Reply

3,386 Views
HyperFrank
Contributor I

Hello, 

I have the exact same problem right now. Did you find a solution?

I tried uninstalling and reinstalling S32DS, but no success  

0 Kudos
Reply