S32K Chip Performance and Motor Control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Chip Performance and Motor Control

ソリューションへジャンプ
2,233件の閲覧回数
zhangchun
Contributor III

hello

I am currently using s32k144 to create a motor controller, but due to the performance impact of s32k144, the motor controller cannot achieve the expected state.

At present, I have used a system frequency of 80M in my code, with O3 as the optimization level, cache enabled, FPU enabled, and fixed-point operations used to improve code execution efficiency.

I want to replace a chip without changing the current code to improve performance, and choose a chip with a higher system frequency and larger cache, among other factors.

excuse me

1. Are there any other optimization plans to improve code performance

2. Do the s32k series chips have the same IP addresses as S32K144's FTM, TRGMUX, PDB, ADC, and have higher performance?

 

Thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
2,189件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried to use AMMClib? This library is very well optimized for motor control. 

jiri_kral_0-1693488234372.pngjiri_kral_0-1693488234372.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,190件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried to use AMMClib? This library is very well optimized for motor control. 

jiri_kral_0-1693488234372.pngjiri_kral_0-1693488234372.png

 

0 件の賞賛
返信
2,182件の閲覧回数
zhangchun
Contributor III
Hi
Thank you very much for your reply,
0 件の賞賛
返信