S32DS3.6.6 Lauterbach plugin returns error message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.6.6 Lauterbach plugin returns error message

Jump to solution
1,719 Views
DirkEtzler
Contributor IV

When using the indicated "Lauterbach" button below within S32DS3.6.6., S32Ds throws an error (exception) message.  Where can I find more information on what the error message means and how to resolve this issue?

Screenshot 2026-03-25 095046.png

Screenshot 2026-03-25 094612.png

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,661 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DirkEtzler,

Try changing the paths under your debug configuration to the actual T32 location. The error you've shared mostly appears when there is no valid T32 installation detected.

Best regards,
Julián

View solution in original post

0 Kudos
Reply
4 Replies
1,697 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DirkEtzler,

Do you have a valid TRACE32 installation? T32 plugin directly calls your local installation, you can refer to the debug configurations:

TRACE32_eclipse.png

You can refer to TRACE32 documentation: TRACE32 Integration to Eclipse.

Best regards,
Julián

0 Kudos
Reply
1,679 Views
DirkEtzler
Contributor IV

Hello @Julián_AragónM,

yes, I do have a valid T32 installation and license.  However, the T32 sits at a non-standard location (e.g., not under C:\T32).  Let me check the documentation in the mentioned link and see if there is guidance on my topic.

Tags (3)
0 Kudos
Reply
1,662 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DirkEtzler,

Try changing the paths under your debug configuration to the actual T32 location. The error you've shared mostly appears when there is no valid T32 installation detected.

Best regards,
Julián

0 Kudos
Reply
1,655 Views
DirkEtzler
Contributor IV

Hello @Julián_AragónM,

My specific debug configurations are working fine.  I have corrected the S32DS path variable for T32 and also edited the corresponding configuration file.  With these changes my Lauterbach is called and the control is transferred over to Lauterbach.

Screenshot 2026-03-26 141722.png

I was just specifically interested what this LB button is being used for and why it is throwing an error?  

Screenshot 2026-03-26 142029.png

I will see if Lauterbach can educate me on their plug-in.  Thank you so far.

Tags (3)
0 Kudos
Reply