S32DS3.5 can not be opened

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS3.5 can not be opened

1,634件の閲覧回数
ruoran_huang
Contributor I

The program has the following error message:

"Incompatibla JVM. Version 1.8.0_202 of the JVM is not suitable for this product. Versoin: 11 or greater is required."

It did not use the installation of the included jre. So I modified s32ds.ini by add "-vm ~~/NXP/S32DS.3.5/jre/bin/javam.exe", the software can be opened, but after that, every time I click on s32ds.exe, the software goes to the loading page, but halfway through the progress bar, the program gets closed unexpectedly with no error message,  and it won't even go to the page where the workspace is selected.
How can this problem be solved, thank you so much!

0 件の賞賛
返信
2 返答(返信)

1,340件の閲覧回数
mabduljawad
Contributor I

I faced the same issue, and I solved by adding the following modification in the s32ds.ini

  • Added "-vm C:/NXP/S32DS.3.5/jre/bin"
  • Modified "-Defxclipse.java-modules.dir=C:/NXP/S32DS.3.5/jre/javafx-sdk-11.0.2/lib"

Then i was able to start the Design Studio without problems.

0 件の賞賛
返信

1,383件の閲覧回数
mabduljawad
Contributor I

I have the same issue, were you able to solve it ?

0 件の賞賛
返信