Hi,
I would like to generate the blob image for SDcard.
The problem is that IVT Tool always displays "The current value if out of range" whenever I set the start address filed in the Application bootloader section. I've tried values from 0 to 4096 and 0x1200 (After IVT image + 512 bytes alignment). All values were not accepted.
And the automatic align shows "The current automatic align start address is causing overflow. The automatic align process is not possible."
My settings are below:
- Processor: S32E270, Green Box3
- Boot target: System Manager M33
- Boot device type: SD/MMC/eMMC
- Turned off all the items in the Image Table section except the Application bootloader.
- IVT image start address 0x1000 => As I know this is fixed.
- In application bootloader section
* Start address : Any value shows "The current value is out of range" in Problem tab.
* Size in bytes: I've entered a value aligned to 8 bytes
What value should I use for the Start address of Application bootloader section.