S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS

1,716 Views
ScottXing
Contributor II

hello experts,there is a issue bothers here: when I Insert a break point into wherever line in whichever project in this work space it looks like this,and the break point can't be active.

I want know that which setting should I change to make the break points can be actived again?

thank y'all and best wishes everybody.

1000010105.jpg1000010105.jpg

0 Kudos
Reply
1 Reply

1,696 Views
IsaulO
NXP Employee
NXP Employee

Hi @ScottXing ,

First of all, check if the "Skip all breakpoints" option is enabled, if so, this causes this behavior, please disable it.

Untitled picture2.pngUntitled picture2.png

BR,
IsaulO

0 Kudos
Reply