S32DS v3.4 + SDK RTM 4.0.2: example project not getting compiled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS v3.4 + SDK RTM 4.0.2: example project not getting compiled

跳至解决方案
2,955 次查看
abhishek_kulkar
Contributor I

Hello Folks!

I have an evaluation board for S32K142.

Downloaded and installed S32 Design Studio for S32 Platform v3.4.

Downloaded and installed S32K SDK RTM 4.0.2.

Opened the Hello World example project from the SDK.

After attempting to build the project, getting this error message:S32DesignStudiov3.4_Problem.JPG

Please suggest what one should do additionally to compile the SDK example projects. Thanks!

0 项奖励
回复
1 解答
2,948 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @abhishek_kulkar,

How did you install S32K SDK RTM 4.0.2? Did you use S32DS Extensions and Updates or did you use Install New Software?

If you use S32DS Extensions and Updates (strongly encouraged option), then it would have required you to also install S32K1xx development package. This development package is required to add necessary support for S32K1xx devices to S32 Design Studio. If you did not install this package, then the build would not work for the example projects.

image.png

Best Regards,

Mike

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,944 次查看
abhishek_kulkar
Contributor I

Hello Mike,

 

Thanks for the quick response, the approach suggested by you worked perfectly!

 

Looking forward to exploring the example software now.

 

Regards,

Abhishek.

0 项奖励
回复
2,949 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @abhishek_kulkar,

How did you install S32K SDK RTM 4.0.2? Did you use S32DS Extensions and Updates or did you use Install New Software?

If you use S32DS Extensions and Updates (strongly encouraged option), then it would have required you to also install S32K1xx development package. This development package is required to add necessary support for S32K1xx devices to S32 Design Studio. If you did not install this package, then the build would not work for the example projects.

image.png

Best Regards,

Mike

 

0 项奖励
回复