S32DS v3.4 + SDK RTM 4.0.2: example project not getting compiled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS v3.4 + SDK RTM 4.0.2: example project not getting compiled

ソリューションへジャンプ
3,029件の閲覧回数
abhishek_kulkar
Contributor I

Hello Folks!

I have an evaluation board for S32K142.

Downloaded and installed S32 Design Studio for S32 Platform v3.4.

Downloaded and installed S32K SDK RTM 4.0.2.

Opened the Hello World example project from the SDK.

After attempting to build the project, getting this error message:S32DesignStudiov3.4_Problem.JPG

Please suggest what one should do additionally to compile the SDK example projects. Thanks!

0 件の賞賛
返信
1 解決策
3,022件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @abhishek_kulkar,

How did you install S32K SDK RTM 4.0.2? Did you use S32DS Extensions and Updates or did you use Install New Software?

If you use S32DS Extensions and Updates (strongly encouraged option), then it would have required you to also install S32K1xx development package. This development package is required to add necessary support for S32K1xx devices to S32 Design Studio. If you did not install this package, then the build would not work for the example projects.

image.png

Best Regards,

Mike

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,018件の閲覧回数
abhishek_kulkar
Contributor I

Hello Mike,

 

Thanks for the quick response, the approach suggested by you worked perfectly!

 

Looking forward to exploring the example software now.

 

Regards,

Abhishek.

0 件の賞賛
返信
3,023件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @abhishek_kulkar,

How did you install S32K SDK RTM 4.0.2? Did you use S32DS Extensions and Updates or did you use Install New Software?

If you use S32DS Extensions and Updates (strongly encouraged option), then it would have required you to also install S32K1xx development package. This development package is required to add necessary support for S32K1xx devices to S32 Design Studio. If you did not install this package, then the build would not work for the example projects.

image.png

Best Regards,

Mike

 

0 件の賞賛
返信