S32DS licence available 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS licence available 0

Jump to solution
3,399 Views
cio74
Contributor I

Hello,

 

I have installed the product in a laptop, it generates one licence? Then trying to install it on a PC, using the same activation code, says no licences available.

 

Fulfillment ID:

120609221

 

How do I fix it?

 

Thanks.

 

Cio

0 Kudos
Reply
1 Solution
3,348 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the number of available licenses has been increased. 

View solution in original post

0 Kudos
Reply
3 Replies
3,349 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the number of available licenses has been increased. 

0 Kudos
Reply
2,222 Views
R_S002
Contributor III

hi @jiri_kral 

i'm also facing same issues

help

0 Kudos
Reply
3,323 Views
cio74
Contributor I

All good now, thanks.

0 Kudos
Reply