S32DS install S32M24x_RTD got error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS install S32M24x_RTD got error

1,281 Views
yuan28149
Contributor I

我正在尝试安装 SW32K1_S32M24x_RTD_R21-11_2.0.0_QLP1_DS_updatesite_D2408,但它失败了,并附加了日志错误文件。

您能帮忙检查一下吗?

Tags (1)
0 Kudos
Reply
2 Replies

1,225 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

如果在线安装RTD失败,请尝试离线安装RTD的方法:HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,242 Views
yuan28149
Contributor I

By the way, the version is 3.5.14.

The suggestion is using 3.5.12, but now the extension can not find this one.

0 Kudos
Reply