S32DS how to properly dump RAM in debug session?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS how to properly dump RAM in debug session?

6,457 Views
embedded_eng
Contributor I

Hello,

I'm using MPC5744P PowerPc architecture uC for development. I'm trying to dump a small block of RAM after using Trace functions in uC/OS-III which is my main OS.

After I dump RAM, it seems like whole RAM is all zeros, but this is impossible.

Can you tell me what is the proper way to dump RAM as bin file?

P.S. I'm using PE Micro Multilink Universal programmer.

Thank you,

Regards

Labels (1)
0 Kudos
Reply
2 Replies

5,957 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, I do not know Trace functions in uC/OS-III, but S32DS has it's own method, how to dump memory.

In debug session, click Memory tab and choose export. Export memory menu will appear. Please see figure below:

pastedImage_1.png

Now choose the required format, address range and path and click OK File with memory dump will be created.

Please let me know if this solution is suitable for you.

Regards,

Martin

5,957 Views
embedded_eng
Contributor I

Hello Martin, thank you for your answer and detailed explanation.

It is working.

I used the same principle, but it seems I chose the wrong export format, and some variables were reseted to zero due to some other functions, so I was getting a wrong data out. I'm using this for uC/OS-III Trace data export.

Thank you again.

0 Kudos
Reply