S32DS for installing RDT errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS for installing RDT errors

ソリューションへジャンプ
1,572件の閲覧回数
Henry_Mei
Contributor III

Hi, 

Have a good day.

Please help to check a S32DS S32R41 RTD package question.

1). Installed S32DS 3.5.0. version: 3.5 Build id: 230226 (Update 2)

2) To download SW32SAF85xx_S32R41_RTD_4.4_0.9.0_HF01_D2211_DS_updatesite.zip

3) Open the S32DS3.5 and go to Help => Install New Software==> Click on the “Add” button.

4) Click on the “Archive” button and look for the SW32SAF85xx_S32R41_RTD_4.4_0.9.0_HF01_D2211_DS_updatesite.zip and add it.

5) When clicking the next button, it has an error. Please refer to the pic below. 

Henry_Mei_0-1688115468093.png

 

Henry_Mei_0-1688116168901.png

 

 

 

Br,

Henry

 

0 件の賞賛
返信
1 解決策
1,527件の閲覧回数
nxf92108
NXP Employee
NXP Employee

Hi @Henry_Mei 

Based on pictures you provided, it is might not be a problem on this package installing. It will be helpful to refer "Show Error Log" and see if this problem is related to your system.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,528件の閲覧回数
nxf92108
NXP Employee
NXP Employee

Hi @Henry_Mei 

Based on pictures you provided, it is might not be a problem on this package installing. It will be helpful to refer "Show Error Log" and see if this problem is related to your system.

 

0 件の賞賛
返信