S32DS  for PowerPC 1.0 Generate Srec file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS  for PowerPC 1.0 Generate Srec file

4,327 次查看
jinjingyang
NXP Employee
NXP Employee

Dear Sir,

 

Customer was able to generate S19 (srec) file in S32DS for PowerPC 1.0 when newly create an MPC5746R project.

And customer gradually add more and more .c and .h files into the project and build. Still OK to generate srec file.

After adding more than 100+ files into the project and build, the srec file is missing.

We can still see the elf file and can still download and debug in S32DS IDE. But just not able to generate an srec file.

 

Do  you know of this kind of problem?

 

Regards,

Jason Yang

标签 (1)
标记 (3)
3 回复数

3,205 次查看
stanish
NXP Employee
NXP Employee

Hi Jason,

Thanks for this report.

Flash image (srec) is created using powerpc-eabivle-objcopy.exe

When "Create flash image" option is enabled (tick it and click on Apply -> new Standard S32DS Create Flash Image settings node appears in the Tools settings)  you should see its output in the build console after the successful build:

pastedImage_2.png

pastedImage_1.png

Is there any error visible in the build console?

They can also try to convert the elf file into s-record using this command line util. manually:

powerpc-eabivle-objcopy.exe -O srec  -v <Path_to_my_elf>\Test_MPC5748G_Z4_0.elf   "Test_MPC5748G_Z4_0.srec"

Can you paste here the console output?

 

Thanks!

Stan

3,205 次查看
jinjingyang
NXP Employee
NXP Employee

Stan,

Thank you for your detailed explanation.

Customer did check those options. I will let them check the console response.

Regards,

Jason Yang

0 项奖励
回复

3,205 次查看
jinjingyang
NXP Employee
NXP Employee

Customer checked the console, there is no such message. But after adding the "powerpc-eabivle-objcopy.exe -O srec" command, they are able to generate s19 file. Thank you for your help.

0 项奖励
回复