S32DS for ARM 2018.R1 Install Anywhere error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for ARM 2018.R1 Install Anywhere error

2,534 Views
AdrianR
NXP Employee
NXP Employee

Hi,

Customer reported repeated failed installs of the S32DS ARM 2018.R1, on his work PC.

The window asking for activation code is not opening in his case, the installation is just falling back and uninstalling itself.

He has run the installer using admin rights.

Looking at the other threads hints, we tried, unsuccessfully:

- installing a newer JRE

- switching network to a PUBLIC one

- moving JRE path upper in the PATH variables

- re-trying in a different folder

Attached is the last installation log failure: - it doesn't say much about the cause:

Install Uninstaller:      S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
                          Status: ERROR
                          Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Any ideas of what to try next are welcome!

Tags (2)
0 Kudos
Reply
1 Reply

2,209 Views
xiehao5
Contributor I

Hi Adrian,

Please check the windows service "Server" status.

Installanywhere relies on the service.

Make sure the "Server" service is enabled and running.

Then retry the installation.

0 Kudos
Reply