S32DS example on Devkit MPC5748G Error in service launch sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS example on Devkit MPC5748G Error in service launch sequence

9,752 Views
uditsalunke
Contributor III

I am trying to program and debug MPC5748G using openSDA #example project - hello (C:\Freescale\S32_Power_v1.1\S32DS\Examples\MPC5748G\hello) on my new devkit MPC5748G.

 

I got bellow error and debug session wont start;  (S32DS version 1.1 and Build ID :160608)

164976_164976.pngpastedImage_1.png

My debugger configuration 

164981_164981.pngpastedImage_3.png

 

Host machine : Win7 64bit running on Intel core i3

 

Can anyone, experienced same issue share how to resolve this? 

is this known issue? 

Labels (2)
14 Replies

8,860 Views
nxppower912935
Contributor IV

Hi all again,

follow up. What's the status of the issue? 

The download works awfully slow to me and then again, it seems not to work - but it did, once, if I remember correctly.

COM port seems available, but trying uart sample I have no look seeing any tx msgs.

There is a maybe related issue report here https://community.nxp.com/thread/441035 - 12V doesn't fix it for me. I'll investigate further.

Best regards

0 Kudos
Reply

8,860 Views
stanish
NXP Employee
NXP Employee

Hello Ludwig

Thanks for the details,

I guess you are not able to connect to the board neither.

The investigation is still in progress. 

We will keep you informed about the progress.

Stan

8,860 Views
tamtran
NXP Employee
NXP Employee

Hello all,

I met the same problem,  Is the investigation of this problem still in progress?...please give me any information you've got.

Thanks and best regards,

Tam.

0 Kudos
Reply

8,860 Views
nxppower912935
Contributor IV

Hi Tam,

I was actually able to download firmware to target, but it's so slow, I makes me wonder. Try a clean restart of your machine, check COM  ports, check USB leads and swap USB cables to be sure there is no issue physically. You need to set the interface in debug in eclipse. Kind regards, LS

0 Kudos
Reply

8,860 Views
tamtran
NXP Employee
NXP Employee

Hi Ludwig,

Thanks for the support,

I think the issue is caused by the board itself because I have 2 boards, one of them that I able to download firmware normally but one met the issue.

Best regards,

Tam

0 Kudos
Reply

8,860 Views
martin_kovar
NXP Employee
NXP Employee

Hello Tam,

the problem, why it was not possible to connect to the board was, that U14 gate QFN was inverted. Please measure U14 gate output voltage (it should be around 3.3V). If you measure something like 1.2V (not correct CMOS logical 1), please contact Ricardo Ruiz Velasco Lomeli <[email protected]>

Regards,

Martin

8,860 Views
tamtran
NXP Employee
NXP Employee

Hi Martin,

I have 3 boards (2 boards fail, 1 board ok). I tried measuring them. The results are:

- Board Ok: the output voltage is 3.3v

- 2 boards Fail: 1 is 3.3v and 1 is 0v. With the board fail 3.3v, it has the same issue with the following link

https://community.nxp.com/thread/395670 

Regards,

Tam

0 Kudos
Reply

8,860 Views
martin_kovar
NXP Employee
NXP Employee

Hello Tam,

if the problem with boards you cannot connect to are related to MPC5748G Flash Problem, (reset occurs while you downloading/erasing the code) please read Lukas Zadrapa's post at this thread https://community.nxp.com/thread/444748 .

Regards,

Martin

0 Kudos
Reply

8,860 Views
nxppower912935
Contributor IV

Hi all,

I wanted to follow-up on the "investigation of the problem or board" before most people are on a holiday break.

Stan, I was able to flash the board, because you wrote I am not able to connect it, however there was something dodgy going on and I was thinking to change the micro-USB cable etc. to make sure everything is electrically all right. Also I am working through a VM (Mac<->Win10), however in 95% all USB devices connected to the VM work as expected.

Regards and happy holidays!

Ludwig

0 Kudos
Reply

8,860 Views
nxppower912935
Contributor IV

Hi all,

which boards are affected?

Mine:

700 - 29030 RevA

SCH - 29030 RevB

L330160167

stanish‌ do you have any news from your side?

Regards,

Ludwig

0 Kudos
Reply

8,859 Views
datamstr
Contributor II

I had the same problem with downloading, then after I connected 12 VDC power, it worked OK.

David

0 Kudos
Reply

8,860 Views
uditsalunke
Contributor III

hello,

Thanks for sharing your observations. I have raised a Support ticket

request to NXP, I got couple of test instructions which I followed and then

its confirmed that there is an issue with the hardware.

Udit

On Tue, Oct 4, 2016 at 8:21 PM, datamstr <[email protected]>

0 Kudos
Reply

8,860 Views
stanish
NXP Employee
NXP Employee

Hello Udit,

Could you please indicate which revision and S/N of the board you have?

There should be some labels at the bottom side of the board:

Devkit_bottom.jpg

Thanks!

Stan

0 Kudos
Reply

8,860 Views
uditsalunke
Contributor III

Stan,

for my board its two labels at back side reads as below 

700 - 29030  RevA

SCH- 29030 RevB

L330160087

Udit