S32DS erases everything in the output folder when building the project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS erases everything in the output folder when building the project

1,021 Views
jimd2023
Contributor I

Hi guys, how can I turn off the feature in S32DS that erases everything in the output folder when building the project as I have some files there like the bootloader hex file and the tools that merge the bootloader with the application hex file and it is really not convenient to copy them back every time?

Thanks in advance for the help 

0 Kudos
Reply
1 Reply

987 Views
mikedoidge
NXP Employee
NXP Employee

Hello Jim,

If you are referring to the folder 'Debug_RAM', for example, then only the files which are a product of the build are erased and replaced. If you rename the files they should remain in the folder.

What version of S32DS are you using?

Best Regards,

Mike

0 Kudos
Reply