S32DS debug error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,659件の閲覧回数
海波张
Contributor I

Error in services launch sequence
Failed to launch GDB server. Please check that another instance of pegdbserver_console.exe is not running.

How to solve the problem, thank you!

タグ(2)
0 件の賞賛
返信
1 解決策
2,372件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

just check if another GDB server is not running via task manager. In windows press CTRL+SHIFT+ESC to start task manager. If there is present pegdbserver process - just kill it. It may happen if for example debug session is interrupted by disconnect from USB or power outage.

Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,372件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

See the answer from Jiri (find and kill the P&E gdb server in the task manager). Otherwise, this article shows it for KDS, but the same principle applies to S32 DS.

Erich

0 件の賞賛
返信
2,373件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

just check if another GDB server is not running via task manager. In windows press CTRL+SHIFT+ESC to start task manager. If there is present pegdbserver process - just kill it. It may happen if for example debug session is interrupted by disconnect from USB or power outage.

Jiri

0 件の賞賛
返信