S32DS debug S32K144 use J-Link tools issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS debug S32K144 use J-Link tools issue

1,948件の閲覧回数
weiq
Contributor I

When using the S32DS software, I used J-LINK to debug the S32K144 development board, but I encountered the following questions and tips. Can you help me?捕获1.PNG

捕获.PNG

configuration is following 

捕获2.PNG

タグ(2)
0 件の賞賛
返信
1 返信

1,866件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi wei,

Please check the jumper setting of J107. If connect 1-2, then you need to power S32K144 by external 12V power source.

J107.png

Have you try to use the on board debug interface? The OpenSDA should be able to debug S32K144 by default.

S32K144EVB-QSG OpenSDA.png

S32K144EVB-QSG OpenSDA (2).png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信