S32DS can not debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS can not debug

4,554 Views
KidhRobin
Contributor II

hello,

I got a issue when I debug  with S32DS . 

I use PE to debug S32K344 mini EVB ,

The board and PE is OK ,I can debug with IAR IDE normally; 

S32DS version:

KidhRobin_2-1698297001390.png

 

I flashed the code (both demo code or myself code), it run to the main,  

KidhRobin_0-1698296602272.png

when I Step into or Step over , it showed like this

KidhRobin_1-1698296744679.png

I tried to re-install the S32DS ,but the issue still exist.

how can I solved this issue?

Thank you very much. 

 

All console  information:

Connection from "127.0.0.1" via 127.0.0.1. Connection from port "65528" to 6224
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "65533" to 7224
Telnet server running on 127.0.0.1:51794
Searching for Kernel Symbols...
rsp_qC - qSymbol: 5F74785F7468726561645F63757272656E745F707472
_tx_thread_current_ptr not found. ThreadX analysis not enabled.
rsp_qC - qSymbol: 707843757272656E74544342
pxCurrentTCB not found. FreeRTOS analysis not enabled.
Unable to load libusb0.dll
Copyright 2023 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS.3.5\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.7.3.202310061729\win32\pegdbserver_console -device=NXP_S32K3xx_S32K344 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port= �
PEmicro Interface detected - Flash Version 11.22

CMD>RE

Initializing.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS.3.5\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.7.3.202310061729\supportFiles_ARM\NXP\S32K3xx\nxp_s32k344_1x32x980k_hse_enabled.arp

Initializing.
Initialized.

;version 1.01, 09/23/2022, Copyright 2022 P&E Microcomputer Systems, www.pemicro.com [S32K3x4_hse_enabled]

;device nxp, s32k344, 1x32x980k,desc=hse_enabled

;begin_cs device=$00400000, length=$003D4000, ram=$20400000

Loading programming algorithm ...

WARNING - Selected .ARP file has been modified. CRC16 = $CF2E
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Command is inactive for this .ARP file.
VC is not implemented, falling back to VM

CMD>VM

Verifying.
Verified.

Application verified in memory. No need to reprogram.

CMD>RE

Initializing.
Target has been RESET and is active.

Starting reset script (C:\NXP\S32DS.3.5\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.7.3.202310061729\supportFiles_ARM\NXP\S32K3xx\S32K344.mac) ...
REM Enable clocks for selected cores in MC_ME module (the sequence below enables all clocks).
REM Initialize RAM and DMA:
REM Initialize DMA TCD:
REM Copy valid executable code to RAM for each core to be used.
REM Enable required cores in MC_ME:
Delaying for 20mS ...
Done.

Reset script (C:\NXP\S32DS.3.5\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.7.3.202310061729\supportFiles_ARM\NXP\S32K3xx\S32K344.mac) completed.

PE-ERROR: Warning. Can't read memory while part is running. @40274040 (12 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @400f00 (64 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @400f38 (2 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @400f24 (2 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @400f14 (2 bytes)
PE-ERROR: Warning. Can't read registers while part is running.

 

0 Kudos
Reply
4 Replies

4,471 Views
KidhRobin
Contributor II

thank you ,this issue had been solved.

I closed the memory related window, it can work normally.

Maybe once before I used these function in a project ,but I do not close these windows ,then when I debug another project ,this error happened; 

I found that even if I delete all the project and then create a new one, I still encounter the same error. Reinstalling S32DS doesn't help either; only after closing these windows, can I work normally.

KidhRobin_0-1698727727046.png

 

0 Kudos
Reply

4,521 Views
juan_see
Contributor III

Hi @KidhRobin ,

 

Could you please create a support request ticket on the PEmicro website? Please click on the "Support Requests" link

https://www.pemicro.com/support/index.cfm

That way, the issue can be investigated by PEmicro engineers. 

0 Kudos
Reply

3,797 Views
Anu_123
Contributor I

Hi ,

I'm also face same issue. 

While I'm flashing the Clock_Ip_Example_S32K344 and Mcu_Example_S32K344 code. 

The Clock_Ip_Example_S32K344 code flashes with no issue. But Mcu_Example_S32K344 shows some error during the flash such as,

  1. PE-ERROR: Warning. Can't read registers while part is running
  2. PE-ERROR: Warning. Can't read memory while part is running

Due to these error, that code does not execute the MCU_SetMode(McuModeSettingConf_0); function.

I closed the memory related windows, still I faced same issue.

Anu_123_1-1722488261371.png

 

 

 

0 Kudos
Reply

3,770 Views
juan_see
Contributor III

Hi @Anu_123 ,

 

I ran a quick test on my S32K3X4EVB-T172 and did not see the "PE-ERROR: Warning. Can't read registers while part is running" that you described. 

I was able to reach the "if (Mcu_GetClockFrequency(CLKOUT_RUN_CLK) != CLOCKOUT_FREQ_CFG_0)" line. 

Can you please try closing the "0x0" file that is open in your view and try launching a debug session again:

Anu_123_1-1722488261371_0x0.png

 

0 Kudos
Reply