S32DS blink LED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS blink LED

5,326 Views
shashankanand
Contributor I

mikedoidge‌

Hi Mike,

Based on your  "HOWTO: Create the Blinking LED example project using S32K144 SDK " I am trying to toggle all the three LEDs on the S32K144EVB_100  but I am not able to do it. 

Following is the code I am running on S32DS:

CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
PINS_DRV_SetPinsDirection(PTD,1<<15U|1<<16U|1<<0U);
PINS_DRV_SetPins(PTD,1<<15U|1<<0U);
PINS_DRV_ClearPins(PTD,1<<16U);
PINS_DRV_SetPins(PTD,1<<16U);

PINS_DRV_ClearPins(PTD,1<<0U);


for(;;){
int c=7200000;
while(c--);
PINS_DRV_TogglePins(PTD, 1<<15U |1<<16U|1<<0U);
}

with this code the toggling is happening between blue and yellow(red+green).

Please help.

Thanks

Shashank Anand

0 Kudos
Reply
2 Replies

3,666 Views
Shrini
Contributor I

turn the led on using switch status...

0 Kudos
Reply

4,587 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

from EVB schematic you can see that LEDs are connected from VDD to GPIO. That means when you Clear pin - LED is ON, when you SET pin - LED is OFF. 

To turn OFF all LEDs - you need to Set particular LED pin. 

You can use OR and SHIFT like: 

PINS_DRV_SetPins(PTD, (1<<16U) | (1<<15U) | (1<<0U) );

or write HEX value 0x18001 (1 10000000 00000001b)

PINS_DRV_SetPins(PTD, 0x18001);

To turn ON all LEDs - you can just switch SetPins to ClearPins

PINS_DRV_ClearPins(PTD, (1<<16U) | (1<<15U) | (1<<0U) );

You can also use only one LED: 

Blue ON:

PINS_DRV_ClearPins(PTD, 1 << 0);

Blue OFF:

PINS_DRV_SetPins(PTD, 1 << 0);

RED ON:

PINS_DRV_ClearPins(PTD, 1 << 15);

RED OFF:

PINS_DRV_SetPins(PTD, 1 << 15);

GREEN ON:

PINS_DRV_ClearPins(PTD, 1 << 16);

GREEN OFF:

PINS_DRV_SetPins(PTD, 1 << 16);

So - in your code you can see that in Init - at the end - you turned OFF GREEN and RED and BLUE by:

PINS_DRV_SetPins(PTD,1<<15U|1<<0U);

PINS_DRV_SetPins(PTD,1<<16U);

and turned ON BLUE by: 

PINS_DRV_ClearPins(PTD,1<<0U);

As you see - in for(;;)

you are toggling between Blue On/Off and (GREEN+RED) On/Off 

because BLUE was ON and GREEN+RED was OFF). 

Jiri