S32DS activation failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS activation failure

2,414 Views
635986562
Contributor I

Hi,  I have installed S32DS(version:S32DS_Vision_Win32_v2018.R1_b181126)in the ubuntu. I  opened  the software and it asked for an activation at first , but I ran into  a problerm like this:

CLLReason[errorNo=21,errorString=Error sending anactivation request to a remote activation server and processiong the resulting response .(FNP errror 50040,41147,10250),flxActMajorErrorNo=50040,flxActMinorErrorNo=41147,flxActSysErrorNo=10250,flxCommErrorNo=0]

I have tried many times,but still can't solve this problem.Can you give me some suggestions?

Thank you very much!

1.png

2.png

0 Kudos
Reply
3 Replies

992 Views
Maka_Zhang
Contributor I

您好,现在解决了吗?当我为 S32 平台 3.5 安装 32 Design Studio 以激活激活码时,向远程激活服务器发送激活请求并处理该服务器时出错,发生了响应。(FNPerror50040、41147102、50),之前下载软件后再关闭,不知道是不是没删干净,再安装一次就卡在这个地方不上去了

加载外部化属性

RepositoryManager:正在尝试回退存储库位置...
==== 安装程序属性日志开始: ====
用户安装目录: D:\NXP\S32DS.3.6.0
用户快捷方式: C:\Users\shyjy01\AppData\Roaming\Microsoft\Windows\Start Menu\Programs\NXP S32 Design Studio\S32 Design Studio for S32 Platform 3.6.0
==== 安装程序属性日志结束。====#

# 安装虚拟机: D:\NXP\S32DS.3.5\jre
#
System's temporary directory = C:\Users\shyjy01\AppData\Local\Temp
==== NET SESSION 命令日志开始: ====
返回: 0
Console: 列表是空的。


错误:
==== NET SESSION 命令日志结束。
许可证服务安装日志开始:====
控制台:找到C:\\Program Files (x86)\\Common Files\\Macrovision Shared\\FlexNet Publisher\\FNPLicensingService.exe
版本
11.18.2.0
找到C:\\Program Files\\Common Files\\Macrovision Shared\\FlexNet Publisher\\FNPLicensingService64.exe
版本
11.18.2.0

错误:
==== 许可证服务安装日志结束。
许可证激活日志开始: ====控制台

错误: CLLReason [errorNo=21, errorString=错误地向远程激活服务器发送激活请求并处理结果响应。(FNP 错误 50040,41147,10250),flxActMajorErrorNo=50040,flxActMinorErrorNo=41147,flxActSysErrorNo=10250,flxCommErrorNo=0]
CLLReason [errorNo=21,errorString=错误向远程激活服务器发送激活请求并处理生成的响应。(FNP 错误 50040、41147、10250)、flxActMajorErrorNo=50040、flxActMinorErrorNo=41147、flxActSysErrorNo=10250、flxCommErrorNo=0]
未输入软件激活码

“=== 许可证激活日志结束。
许可证列表开始: ====控制台

错误:
==== 许可证列表结束。
FNP 库版本日志开始: ====控制台
: PrintFlexVersion.execute()

0 Kudos
Reply

2,246 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I never saw this error message before. What is the last character (probably some unicode stuff) in our activation key? 

Jiri 

0 Kudos
Reply

984 Views
Maka_Zhang
Contributor I
hi, you mean Activation Code? It's not the same version but I'm having the same problem
0 Kudos
Reply