S32DS Unable to add MCAL component

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Unable to add MCAL component

1,370 Views
viswa_kondapall
Contributor IV

Hi,

I am Working LIN- project. Adding LIN-43-LLCE in MCAL. This i am adding in CAN2CAN project which NXP LLCE example project:

viswa_kondapall_1-1681394083783.png

How to add LIN-43-LLCE which is already added with LLCE-1.0.4. 

How to added clock reference :

viswa_kondapall_2-1681394344579.png

 

Regards,

Viswa

 

 

Tags (1)
0 Kudos
Reply
1 Reply

1,337 Views
nxf92355
NXP Employee
NXP Employee

Hi Viswa

Hope you are doing well.

You are using Can_Llce_DS_Can2Can_S32G274A_M7 example which is configured for can. and you are adding Lin component in this example. you have to config Lin_43_LLCE. for this you can refer example Lin_Llce_DS_S32G274A_M7. 

To add clock reference change Mcu Clock Frequency Select as LIN_BAUD_CLK. to change this go to Mcu_1 component  and change Mcu_1 -> McuModuleConfiguration  -> McuColckSettingConfig ->  McuClockReferencePoint. set McuClockReferencePoint_3 as LIN_BAUD_CLK.

Screenshot (23).png

now you will see clock reference error has been resolved .

Screenshot (24).png

 

Regards ,

Tushar

0 Kudos
Reply