S32DS S32 Configuration Tools R1.8.8 NPI data package for S32G3 インストールエラー

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS S32 Configuration Tools R1.8.8 NPI data package for S32G3 インストールエラー

2,265 Views
jmy
Contributor II

S32DS 3.6.6をインストール後、S32 Configuration Tools R1.8.8 NPI data package for S32G3をインストールする途中でエラーが表示されます。

コンフィグツールインストール時エラー2.png

 

コンフィグツールインストール時エラー3.png

アンインストールし、S32DS関連のフォルダを削除後、再度インストールしてもエラーとなります。

原因、改善方法を教えていただけないでしょうか?

 

 

0 Kudos
Reply
7 Replies

2,167 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @jmy,

Your message was automatically translated to English by the community. If you notice a misinterpretation on my side please let me know.

Regarding your issue, I was able to install the packages only after installing the RTD for the S32G, I tested with version 5.0.0:

Screenshot 2026-04-06 152605.png

 

Have you installed the RTD before the NPI Package for S32G3?

 

Please let me know if you have more questions.

Thanks

0 Kudos
Reply

2,031 Views
jmy
Contributor II

Thank you for your reply.
I will write in English.

When I installed S32 Configuration Tools R1.8.8 NPI data package for S32G3, RTD4.0.0 was automatically installed.
Therefore, I did not install RTD before installing the NPI package.

 

Originally, I was able to install S32 Configuration Tools R1.8.8 NPI data package for S32G3 without any errors and it worked without problems.

However, after installing the LLCE firmware and generating the LLCE LIN sample program, errors occurred in the configuration tool's peripherals, and errors also appeared in the source code.

Upon investigation, I found information indicating that LLCE firmware requires RTD4.0.2. Since I had RTD5.0.0 installed in my environment,
I planned to uninstall S32DS, reinstall it, and then install RTD4.0.2.

After uninstalling and reinstalling, when I tried to install S32 Configuration Tools R1.8.8 NPI data package for S32G3, errors occurred.

 

An error has occurred, but the S32 Configuration Tools R1.8.8 NPI data package for S32G3 and RTD4.0.0 are installed. However, it is unclear whether they were installed correctly.

I would like to avoid ignoring the error and continuing to use the current environment.

What are some ways to resolve this error?

Tags (1)
0 Kudos
Reply

2,010 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello again @jmy, 

You can use Japanese if you prefer, the community has an automatic translation tool and I actually see the message in English. In any case I will reply in English.

I understand, however, you should not need to install the NPI data package, the S32DS 3.6.6 has the S32G development package by default. That should include all the tools needed to work with the S32G. I checked the LLCE 1.0.11 release notes and they should be compatible with RTD 5.0.0 QLP3:

alejandro_e_1-1776383695891.png

 

This means you should be able to use LLCE 1.0.11 after installing RTD 5.0.0 + QLP1 + QLP3. 

However, I tried to install RTD 5.0.0 + QLP1 + QLP3 and adding LLCE 1.0.11, and even thought I was able to install all packages without problems, I tried compiling an example and there seems to be a problem with the version required by the LLCE and that breaks the compilation.

I will try to find a workaround and let you know if I can build an example.

 

I will get back to you once I have a relevant update.

Regards

0 Kudos
Reply

1,999 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello again @jmy,

Can you help me by creating a private support ticket, there is some information I need to share that need to be private. Please go to https://www.nxp.com/ , click on "My NXP Account" and then on "My support tickets":

alejandro_e_0-1776471150591.png

 

Please add the link to this post so we can ensure I continue the topic.

 

Thanks in advance and sorry for the inconveniences.

 

0 Kudos
Reply

1,695 Views
jmy
Contributor II

申し訳ございません。マイサポートチケットをクリック後の操作を教えていただけないでしょうか。

NPIデータパッケージをインストールしないと、コンフィグツールが使用できなかった為、NPIデータパッケージをインストールしました。
また、私が入手したLLCEファームウェアのバージョンは1.0.9です。

0 Kudos
Reply

1,671 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @jmy,

Sorry, since I do not use that flow to create ticket I pointed to the incorrect option. You should use the following:

alejandro_e_0-1778710967481.png

Then you should be able to create a ticket with this option:

alejandro_e_1-1778711031873.png

 

 

 Also, you can follow this video, the view may differ a bit, however, the general process is the same: Tutorial for NXP Support Case Portal.

Please remember to add the link to this post so we can be sure I follow the topic.

 

Thanks.

 

0 Kudos
Reply

1,653 Views
jmy
Contributor II

ご連絡ありがとうございます。
マイサポートチケットを作成しました。