S32DS-Pwr - Invalid project path (MPC5777)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS-Pwr - Invalid project path (MPC5777)

Jump to solution
4,990 Views
felixaertz
Contributor I

Hi

I am using S32 Design Studio for Power Architecture, Version: 2017.R1, Build id: 171018 together with PEmicro Multilik Universal FX. Running on Win10 Version 1803 for x64 with latest update (2018-11-19).

Target platform is the MPC5777C.

I did a project some month ago that worked well. Now I want to continue working with the test program, but it is not compiling any more. :smileyplain:

Warnings:
Invalid project path: Referenced project is not accessible.    test_5777_Z7_0        pathentry    Path Entry Problem

... together with...

11:02:40 **** Incremental Build of configuration Debug for project test_5777_Z7_0 **** make -j4 all 3 [main] make 9800 child_info_fork::abort: C:\NXP\S32DS_Power_v2017.R1\utils\msys32\usr\bin\msys-gcc_s-1.dll: Loaded to different address: parent(0x1C0000) != child(0x1A0000) make: fork: Resource temporarily unavailable 11:02:40 Build Finished (took 188ms)

I have cheked the Project -> Properties -> ... Build Variables like project path etc. but everything looks normal.

Does anybody has an idea what's going wrong?

Thanks and best regards

Felix

Tags (2)
0 Kudos
Reply
1 Solution
4,686 Views
felixaertz
Contributor I

Hi,

thanks for the response. The latest windows update (2018-11-29 KB4467682) solved the problem over the weekend.

Win10 is a nightmare in my view...

Best regards

Felix

#closed

View solution in original post

0 Kudos
Reply
3 Replies
4,687 Views
felixaertz
Contributor I

Hi,

thanks for the response. The latest windows update (2018-11-29 KB4467682) solved the problem over the weekend.

Win10 is a nightmare in my view...

Best regards

Felix

#closed

0 Kudos
Reply
4,686 Views
b48014
NXP Employee
NXP Employee

Hi,

The link below could help you

Make error (msys-iconv-2.dll) in Win10 

BR,

Dmitry

0 Kudos
Reply
3,253 Views
allenZhu
Contributor I

hi, I have the same problem as the first one, but I didn't find the answer in this post, what should I do?

allenZhu_0-1705994939086.png

 

0 Kudos
Reply