S32DS Processor Expert Signal Names

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Processor Expert Signal Names

Jump to solution
3,295 Views
martinthompson
Contributor III

Hi everyone & apologies if this is a dumb question...

Is it possible for the pin/signal name defined in the pin_mux component to appear as a #define in the generated pin_mux.h file?

e.g. I have PTA0 with User Pin/Signal Name "RESETM_H".  After generating the Processor Expert code, pin_mux.h contains the following comments

/* ###################################################################
** This component module is generated by Processor Expert. Do not modify it.
** Filename : pin_mux.h
** Project : my_project
** Processor : S32K144_100
** Component : PinSettings
** Version : Component 1.2.0, Driver 1.4, CPU db: 3.00.000
** Repository : SDK_S32K14x_09
** Compiler : GNU C Compiler
** Date/Time : 2018-06-28, 10:56, # CodeGen: 51
** Abstract :
**
** Settings :

** Peripheral Type GPIO :
** Custom name : PTA
** PTA :
** Pin 0 : RESETM_H
** Direction : Output

*/

However, there are no #defines to identify PTA0 as "RESETM_H".  Do I really have to define the port and pin for each GPIO manually???

Thanks in advance

--Martin

S32 Design Studio version 2018.R1, build ID 180504

S32K144 using S32K14x EAR SDK v0.8.6.  

1 Solution
3,086 Views
jiri_kral
NXP Employee
NXP Employee

Hi Martin, 

it is strange - but it looks like that you really need to define custom names by yourself. In my opinion in this case the custom name is unusable in this way. I'll discuss it with SDK team and rise Feature add/or bug ticket. Thank you for report. 

Jiri  

View solution in original post

3 Replies
3,086 Views
ruudsiebierski
Contributor III

Hi,

Any update on this issue? 

Ruud

0 Kudos
Reply
3,086 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

Based on JIRA ticket - the Issue is already resolved. Will be added probably in next SDK release. 

Jiri 

3,087 Views
jiri_kral
NXP Employee
NXP Employee

Hi Martin, 

it is strange - but it looks like that you really need to define custom names by yourself. In my opinion in this case the custom name is unusable in this way. I'll discuss it with SDK team and rise Feature add/or bug ticket. Thank you for report. 

Jiri