S32DS Power2017.R1 Linux version Bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Power2017.R1 Linux version Bug

4,665 Views
willfansh
Contributor I

I use S32DS Power2017.R1 Linux version for MPC5741P development

when I add adc_pal or flexcan components to project

the component inspector page show Extension CTU Prescaler  : No type specified error

PE clock source: No type specified error

....

0 Kudos
Reply
1 Reply

4,591 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, any SDK examples cannot be used in Linux version, because SDK is not supported in Linux so far.

If you want to use SDK, please install Windows version.

Thank you for understanding.

Regards,

Martin

0 Kudos
Reply