S32DS, MPC5777C and PIT interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS, MPC5777C and PIT interrupt

2,462 Views
robertfromcummi
Contributor II

I try to use PEmicro with MPC5777C on S32DS and I cannot generate interrupt from PIT when in debug mode. What should I check?

Labels (2)
0 Kudos
Reply
2 Replies

1,901 Views
stanish
NXP Employee
NXP Employee

Robert ,

FYI: This is a known issue with PIT freeze mode bit (ENGR00379206).

When there is a freeze mode activated the debug run does not trigger start of a timer/peripheral.

Please disable freeze bit as a workaround.

This issue should be addressed in a next release.

Stan

0 Kudos
Reply

1,901 Views
stanish
NXP Employee
NXP Employee

Hello Robert,

I'd recommend you to download and check PinToggleStationery for MPC5777M since it includes PIT interrupt.

Example MPC5777M PinToggleStationery S32DS

Stan

0 Kudos
Reply