S32DS For Power v1.1 Debug problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS For Power v1.1 Debug problem

3,353 Views
eautopower
Contributor IV

There is a error,like:

pastedImage_1.png

I have already reloade  the S32DS ,but the problem remains unsolved.

please tell me what can I do?

0 Kudos
Reply
5 Replies

3,045 Views
stanish
NXP Employee
NXP Employee

Hello,

I'd strongly recommend you to install the latest version of S32DS for Power v1.2 + updates.

Please check the announcements below:

S32 Design Studio for Power v1.2 (Windows/Linux) released! 

https://community.nxp.com/docs/DOC-335067 

Is this still the problem?

Regards,

Stan

0 Kudos
Reply

3,045 Views
eautopower
Contributor IV

hello,

yes,this is still the problem.

0 Kudos
Reply

3,045 Views
stanish
NXP Employee
NXP Employee

Hi,

This is Pemicro GDB server crash. It seems there is an interference with another process. Could you possibly try to run GDB server in standalone mode. Let's assume you have S32R274 target.

Run GDB server:

<S32DS_Power_v1.2>\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.9.201706282002\win32\pegdbserver_power_console.exe -startserver -device=S32R274 

you should observe something like this:

pastedImage_282.png

Are you able to start GDB server without IDE on your side?

0 Kudos
Reply

3,045 Views
eautopower
Contributor IV

Incompatible with the WIN10 X64 system,it is ok now

0 Kudos
Reply

3,045 Views
eautopower
Contributor IV

Hi:

 I tried to turn it on, but exit quickly when it started running

0 Kudos
Reply