S32DS Build error: Program "make" not found in Path, powerpc-eabivle-gcc g++ not found in PATH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Build error: Program "make" not found in Path, powerpc-eabivle-gcc g++ not found in PATH

6,356 Views
ChenBowen
Contributor II

1.png

mpc5744 ,S32DS v2017 .  Someone else provide me with this project, but l build with error "powerpc-eabivle-gcc/g++ not found in PATH , make not found in PATH ".   The other projects all build successfully but only this one fails, why?

 

 

0 Kudos
Reply
6 Replies

6,346 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the project is probably for different version of S32DS for Power Architecture (Probably for the newer  S32ds for Power Architecture v.2.1. Did you Import this project into workspace (on main menu bar File -> Import -> General -> Existing project into workspace). 

 

You can download latest S32DS here:

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

 

 

0 Kudos
Reply

6,335 Views
ChenBowen
Contributor II

I have tried to build the project  both in the v2.1 version and v2017 version,  all happened with such build errors

0 Kudos
Reply

6,331 Views
mikedoidge
NXP Employee
NXP Employee

Was the project provided as a package of just the project directory, or also the workspace?

Make sure you are using a fresh workspace and import the project to that fresh workspace from the original location of the project (as it was provided to you).

The workspace should be replaced each time a new version of S32 Design Studio is used. The old workspace will contain settings which work only for the version of S32 Design Studio from which it created it.

0 Kudos
Reply

6,295 Views
ChenBowen
Contributor II

Also,l have refreshed the WorkSpace for many times ,it doesn't work.

0 Kudos
Reply

6,296 Views
ChenBowen
Contributor II

I  try to click  Properties - Environment- PATH, changed this project's environment variables "PATH" to the same as the other projects .  And now comes another error, please see pictures below. 

ChenBowen_2-1649326295535.pngChenBowen_3-1649326305508.png

How to slove this problem? 

 

 

0 Kudos
Reply

6,287 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

the srec_cat.exe tool is not part of S3DS - this tool is probably called by some post build step - you need to install it by yourself.  

 

Jiri

0 Kudos
Reply