S32DS ADC configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS ADC configuration

ソリューションへジャンプ
1,191件の閲覧回数
LavanyaR
Contributor I

Hi,

I have created the application project in s32k324. I tried to configure the PTE11 pi as an ADC. But in S32DS pin configuration showing default selection. If i select this pin means it doesn't generate the pin configuration in Siul2_Port_Ip_Cfg.h file. Kindly guide me to configure the ADC pin.

LavanyaR_0-1702528084528.png

タグ(1)
0 件の賞賛
返信
1 解決策
1,169件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

You don't need to select those default selection pins in Pins tool.(It will not generate the pin configuration in Siul2_Port_Ip_Cfg.h file)

Please select Adc Physical Channel Name in Peripheral tool.

Adc Physical Channel Name.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,170件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

You don't need to select those default selection pins in Pins tool.(It will not generate the pin configuration in Siul2_Port_Ip_Cfg.h file)

Please select Adc Physical Channel Name in Peripheral tool.

Adc Physical Channel Name.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信