[S32DS 3.4] S32FlashTool for S32G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32DS 3.4] S32FlashTool for S32G

ソリューションへジャンプ
3,665件の閲覧回数
masatakayakashi
NXP Employee
NXP Employee

Hi,

A Debug tool vendor who is working for S32G is asking question about S32FlashTools.
They would like to perform Read/Write/Erase Flash by loading S32G2xxx.bin and MX25UW51245G.bin on SRAM via JTAG debugger. Is it possible? If yes, following questions are popped up.
Q1: Which address should they be stored in?
Q2: Which address is starting address?
Reading MX25UW51245G.bin, they found the address of FA_Init() and FA_ExecCmd(). Should they call FA_Init()? If so, the What value of argument "apParams" for FA_Init should be configured?
Q3: After calling FA_Init(), should they call FA_ExecCmd()?

Best Regards,
Masataka Yakashiro

0 件の賞賛
返信
1 解決策
3,649件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @masatakayakashi,

We have a document regarding the command line use of the Flash Programmer within the S32 Debugger. It uses JTAG connection with S32 Debug Probe.

https://community.nxp.com/t5/INTERNAL-S32-Design-Studio/HOWTO-Command-Line-JTAG-flash-programming-wi...

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,640件の閲覧回数
masatakayakashi
NXP Employee
NXP Employee

Thanks, I will recommend to try S32Debugger.

BR

Masataka 

0 件の賞賛
返信
3,650件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @masatakayakashi,

We have a document regarding the command line use of the Flash Programmer within the S32 Debugger. It uses JTAG connection with S32 Debug Probe.

https://community.nxp.com/t5/INTERNAL-S32-Design-Studio/HOWTO-Command-Line-JTAG-flash-programming-wi...

Best Regards,

Mike

0 件の賞賛
返信