S32DS 1.3 for ARM Export to IAR project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS 1.3 for ARM Export to IAR project

3,742 Views
stevesun
NXP Employee
NXP Employee

Hi,

 

I am using S32DS 1.3 for ARM on S32K projects and would like to use IAR to do the compile and debug. Have tried to right click on the project and select export. However nothing happens when clicking the Finish button, no xml is generated.

 

Could you kindly help advise how I can generate the xml correctly?

 

Thanks!

Regards,

Steve

Labels (2)
Tags (3)
0 Kudos
Reply
3 Replies

3,075 Views
stanish
NXP Employee
NXP Employee

Hello Steve,

I'd recommend you to install IAR plugin into S32 Design Studio. This way you can build and debug your project using IAR tools from S32 Design Studio Eclipse IDE.

See attached screenshots 

Hope it helps.

Stan 

3,075 Views
buckzheng
Contributor II

Hi Stan,

I have installed IAR plugin into S32 Design Studio, I can't build and debug your project using IAR tools from S32 Design Studio Eclipse IDE.When I debug my project ,the debug window remains in S32DS. 

And I want to debug my project in IAR,but this way has no effect.

Additions, I can't watch variables and expressions when the target is running In S32DS Debug window,

Can you give me some suggestions about this problem.

 

And I don't know how to create a  project of S32K144 in IAR, Can you provide me some S32K144 demos In IAR environment. 

pastedImage_1.png

pastedImage_2.png

Regards,

Hunter

0 Kudos
Reply

3,075 Views
stevesun
NXP Employee
NXP Employee

Hi Stan,

Thanks, that's helpful!

Regards,

Steve

0 Kudos
Reply