S32CT from command line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32CT from command line

2,345 Views
pekor
Contributor II

Hello community,

Is there any possibility to use S32 Configuration Tool without launching S32DS IDE v3.4 (using CLI)?

I saw something in "Help contents" of S32DS

pekor_0-1613654954229.png

But first of all there is no executive file besides s32ds in my installation. 
I tried to use the parameters with s32ds.exe, but with no success. IDE is launching normally.

Is it possible or I just do something wrong?

 

 

0 Kudos
Reply
1 Reply

2,305 Views
mikedoidge
NXP Employee
NXP Employee

Hello @pekor ,

You are correct, the command should use the 's32ds.exe'.

I was able to perform the following command without the IDE UI launching:

C:\NXP\S32DS.3.4\eclipse>s32ds.exe -noSplash -consoleLog -application com.nxp.swtools.framework.application -HeadlessTool Peripherals -Load C:\Users\<userid>\workspaceS32DS.3.4\S32CT_commandline\S32CT_commandline_M7_0\S32CT_commandline_M7_0.mex -ExportSrc C:\s32ctgen

I created an empty project 'S32CT_commandline_M7_0' from within S32DS IDE UI and added a driver from the Peripherals tool and generated the code. Then I used the above command to generate the code again to the 'C:\s32ctgen' folder. There was no output to the screen, but the code was generated in the s32ctgen folder as expected. If you want to see the log of the command, you can edit the 's32ds.ini' file located in 'C:\NXP\S32DS.3.4\eclipse' folder and add to the end of the file:
-Djava.util.logging.config.file=configuration/logging.properties

Then you can look for the log file in 'C:\Users\<userid>\.nxp\swtools.log'

Hope it helps,

Mike

0 Kudos
Reply