S32 pemicro port connection error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 pemicro port connection error

1,747件の閲覧回数
cristianchacha
Contributor III

Hello,

I try to use S32 Desing studio in linux, process compilation is ok, but when I want debug with PEmicro , I have a problem with port connection. 

cristianchacha_0-1695044156012.png

From time to time, the connection is succesfully because port number connection change in each connection, but I need to try over and over again, so if there any parameter to configure port number.

I mean "44542" and "60484" , could be statically values ? In my windows machine I saw that correct values are 55778 and 55780 , and every time use these. 

Thanks a lot.

 

タグ(2)
0 件の賞賛
返信
1 返信

1,651件の閲覧回数
juan_see
Contributor III

Hi @cristianchacha , 

Could you please visit the pemicro website and submit a support request there? That way, the issue can be investigated by the PEmicro team directly. 

 

Thanks,

Juan See

PEmicro

0 件の賞賛
返信