S32 for Power - Compatibility with NXP Motor Control Toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 for Power - Compatibility with NXP Motor Control Toolbox

ソリューションへジャンプ
3,841件の閲覧回数
chosp
Contributor III

Hello

 

We are successfully developing on the MPC5744P using S32 Design Studio and PE Multilink.

The NXP Motor Control Toolbox for MATLAB was downloaded for evaluation purposes, but the S32 toolchain is not available among the configurable toolchain choices regarding code generation.

 

Is support for the S32 IDE planned? If yes, do you have an approximate timeline?

 

Thank you

ラベル(1)
1 解決策
3,649件の閲覧回数
PatrickMenter
NXP Employee
NXP Employee

The support for the MC Toolbox for MPC5744P to support the GCC compiler in S32 Design Studio is planned for later this year. The larger target plan is to add this support in late Q3 or early Q4.

元の投稿で解決策を見る

1 返信
3,650件の閲覧回数
PatrickMenter
NXP Employee
NXP Employee

The support for the MC Toolbox for MPC5744P to support the GCC compiler in S32 Design Studio is planned for later this year. The larger target plan is to add this support in late Q3 or early Q4.