S32 design studio version 3.5 setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio version 3.5 setup

1,131 Views
karthickvenkadesh
Contributor I

Hello,

I am using RTD 4.0.0 P19 version and NXP team is suggesting for S32 Design Studio for S32 platform version 3.5. Can you please share me the setup file for S32DS version 3.5.

 

Thanks in advance!

0 Kudos
Reply
1 Reply

1,108 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to the method mentioned in RTD 4.0 with Design Studio 3.5

The last step is to install: SW32K3_S32M27x_RTD_R21-11_4.0.0_P19_D2403_DS_updatesite.zip


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply