S32 design studio version 3.5 setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 design studio version 3.5 setup

1,089件の閲覧回数
karthickvenkadesh
Contributor I

Hello,

I am using RTD 4.0.0 P19 version and NXP team is suggesting for S32 Design Studio for S32 platform version 3.5. Can you please share me the setup file for S32DS version 3.5.

 

Thanks in advance!

0 件の賞賛
返信
1 返信

1,066件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to the method mentioned in RTD 4.0 with Design Studio 3.5

The last step is to install: SW32K3_S32M27x_RTD_R21-11_4.0.0_P19_D2403_DS_updatesite.zip


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信