S32 Design tool Launching issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design tool Launching issue

跳至解决方案
549 次查看
KarthickArumin
Contributor I

Hello Community,

As I am start to work with NXP s32 design studio IDE for my Clients32_IDE.png project, I have installed s32 IDE after installation I trying to open the IDE,but facing the issue. Kindly help me on this Please find the attachment. 

0 项奖励
回复
1 解答
524 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @KarthickArumin 

The issue you are encountering seems to be related to an installation problem. To help diagnose this, it would be useful to review the installation logs from both the base tool and any associated packages.

You can find the installation logs in the following directories:
- C:\NXP\S32DS.3.6.0\_S32 Design Studio for S32 Platform 3.6.0_installation\Logs\S32_Design_Studio_for_S32_Platform_3.6.0_Install_MM_DD_YYYY (date)_HH_MM_SS(time).log
- C:\Users\workspaceS32DS.3.6\.metadata\.log

If you prefer, you can also try reinstalling S32 Design Studio to resolve the issue.

 

BR, VaneB

在原帖中查看解决方案

0 项奖励
回复
1 回复
525 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @KarthickArumin 

The issue you are encountering seems to be related to an installation problem. To help diagnose this, it would be useful to review the installation logs from both the base tool and any associated packages.

You can find the installation logs in the following directories:
- C:\NXP\S32DS.3.6.0\_S32 Design Studio for S32 Platform 3.6.0_installation\Logs\S32_Design_Studio_for_S32_Platform_3.6.0_Install_MM_DD_YYYY (date)_HH_MM_SS(time).log
- C:\Users\workspaceS32DS.3.6\.metadata\.log

If you prefer, you can also try reinstalling S32 Design Studio to resolve the issue.

 

BR, VaneB

0 项奖励
回复