I am struggling to run a project on S32DS for Power ver 1.2, build ID: 170613.
I have a single function "sysclk_init" that is called in main. This only initializes the fmpll. there are no interrupts enabled.
When I step through the code, on entering this function an exception is thrown. Depending on "sysclk_init" is called before or after "xcptn_xmpl()" function, different errors are thrown- (console1.png,console2.png)
I am using PE micro USB multilink.
The debugger settings is attached (debug_settings.PNG).
Also attached is the project.
I have gone through the below links, but could not arrive at a solution after implementing the changes mentioned.
https://community.nxp.com/docs/DOC-335361
https://community.nxp.com/thread/433305
https://community.nxp.com/docs/DOC-335361
Any pointers to move forward?
Any working examples for MPC5634M ON S32 DESIGN studio is available?
Sincerely,
Arjun
Hello,
I tested your use case and I reproduced the same behavior as you described above. Unfortunately, I was not able to find out the root cause, but I think, there is some issue with debugger, because with Lauterbach debugger, the code works correct. There is no reason, why the code should not work.
So, I escalated this issue to application team and now I wait for additional information. Please be patient, I will keep you inform as soon as I have any information for you.
Regards,
Martin
Hello Martin,
Thanks a lot for the actions.
As directed, I will wait for a reply from your side.
Have a nice day.
Hello Arjun,
Thanks for the report. The issue is probably located in the startup script file s32e200_mpc563xm_vle.mac:<S32DS_Power_v2017.R1>\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&E\s32e200_mpc563xm_vle.mac
line 63 is missing instruction:
execute_opcode $7C0007A4 ; tlbweThis causes the MMU page for Perpheral registers A is not configured at all and it throws an exception when accessing the registers.
Attached is the fixed script for your convenience.
Hope it helps.
Stan
Hello Stanish,
Thanks a lot for your answer.
Your solution has worked like a charm and I am able to get my project up and running.
Thanking you for your time and efforts in quick debugging and coming up with a solution.
Wishing you a very nice day,
Arjun.