S32 Design Studio with S32K144EVB-Q100X on Linux missing basic includes for board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio with S32K144EVB-Q100X on Linux missing basic includes for board

2,788 Views
wsmith
Contributor I

S32 Design Studio with S32K144EVB-Q100X, is missing includes like Cpu.h, clockMan1.h, pin_mux.h, which are obviously needed for the board. I am running it in Linux. With find, I don't see those files anywhere in my workspace nor in my installation directory. I am working with the blinking LED example, trying to get that to build.

What am I missing and how do I install it?

Thanks,

William

0 Kudos
Reply
3 Replies

2,552 Views
stanish
NXP Employee
NXP Employee

Hello William,

Thanks for your report. This is probably related to this question:

Processor Expert Window Not Visable S32DS ARM 1.3 Linux 

Stan

0 Kudos
Reply

2,552 Views
wsmith
Contributor I

That is true - I noticed that. The processor expert window does not open in Linux, but if you right click on the .pe file, and choose "Open with text editor" you can at least view the XML.

0 Kudos
Reply

2,552 Views
wsmith
Contributor I

Never mind, I got it. I seemed to have not noticed the part in the video where it says to run "Generate Processor Expert Code".

0 Kudos
Reply