S32 Design Studio for S32 Platform 3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform 3.5

ソリューションへジャンプ
4,170件の閲覧回数
chuanlin
Contributor III

chuanlin_0-1686904218148.png

Hello, using PE for debugging download, what is the reason for this problem

0 件の賞賛
返信
1 解決策
4,065件の閲覧回数
chuanlin
Contributor III

Just change the workspace. Thank you。

元の投稿で解決策を見る

6 返答(返信)
4,124件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @chuanlin ,

The error seems to indicate that S32DS3.5 is not able to find the gdb client. (Or probably missing command gdb launch in debug configuration.) The gdb client is specified in the debug configuration. Please check that the default setting is as below: 

Mehul_Patel_NXP_0-1687792608641.png

Please can you check and get back. 


Thank you, Best regards, 

- Mehul Patel  

 

0 件の賞賛
返信
4,108件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi, @Mehul_Patel_NXP 

    Such issue was met under Windows-11.
    Can you help to confirm whether S32DS_3.5 could run under Win11 correctly?
Thanks
Oliver

0 件の賞賛
返信
4,031件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @OliverTian , 

Sorry for the late reply. 

Is the issue still persist? 

Please can you provide more information to understand the issue. 

Thank you. Best regards. 

- Mehul 

 

0 件の賞賛
返信
4,001件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi, Mehul
   I re-installed WIN10 to overcome such issue. No more test under WIN11 after met such issue.
Hope WIN11 is supported and listed on the introduction of S32DS_3.5 in www.nxp.com 

Regards
Oliver

0 件の賞賛
返信
4,003件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi, Mehul
     I re-install WIN10 to overcome such issue.  No more test on WIN11 after met such issue. 
     Hope WIN11 could be supported and listed on S32DS_3.5's introduction in www.nxp.com

Regards
Oliver

0 件の賞賛
返信
4,066件の閲覧回数
chuanlin
Contributor III

Just change the workspace. Thank you。