S32 Design Studio for S32 Platform 3.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design Studio for S32 Platform 3.5

跳至解决方案
4,137 次查看
chuanlin
Contributor III

chuanlin_0-1686904218148.png

Hello, using PE for debugging download, what is the reason for this problem

0 项奖励
回复
1 解答
4,032 次查看
chuanlin
Contributor III

Just change the workspace. Thank you。

在原帖中查看解决方案

6 回复数
4,091 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @chuanlin ,

The error seems to indicate that S32DS3.5 is not able to find the gdb client. (Or probably missing command gdb launch in debug configuration.) The gdb client is specified in the debug configuration. Please check that the default setting is as below: 

Mehul_Patel_NXP_0-1687792608641.png

Please can you check and get back. 


Thank you, Best regards, 

- Mehul Patel  

 

0 项奖励
回复
4,075 次查看
OliverTian
NXP Employee
NXP Employee

Hi, @Mehul_Patel_NXP 

    Such issue was met under Windows-11.
    Can you help to confirm whether S32DS_3.5 could run under Win11 correctly?
Thanks
Oliver

0 项奖励
回复
3,998 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @OliverTian , 

Sorry for the late reply. 

Is the issue still persist? 

Please can you provide more information to understand the issue. 

Thank you. Best regards. 

- Mehul 

 

0 项奖励
回复
3,968 次查看
OliverTian
NXP Employee
NXP Employee

Hi, Mehul
   I re-installed WIN10 to overcome such issue. No more test under WIN11 after met such issue.
Hope WIN11 is supported and listed on the introduction of S32DS_3.5 in www.nxp.com 

Regards
Oliver

0 项奖励
回复
3,970 次查看
OliverTian
NXP Employee
NXP Employee

Hi, Mehul
     I re-install WIN10 to overcome such issue.  No more test on WIN11 after met such issue. 
     Hope WIN11 could be supported and listed on S32DS_3.5's introduction in www.nxp.com

Regards
Oliver

0 项奖励
回复
4,033 次查看
chuanlin
Contributor III

Just change the workspace. Thank you。