S32 Design Studio for Power with eCos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power with eCos

4,353 Views
antoniograu
Contributor II

Hi,

 

I installed the IDE today and int looks good.

I´m currently using eCos as embedded OS and compiling it with eclipse on Ubuntu and a modified GNU compiler from Sourcery (powerpc-eabi).

 

Do you have a project example to compile eCos with this new S32 Design in windows?

 

Is there a plan to support MPC5668E Processor???

 

Kind regards,

Antonio

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

3,950 Views
stanish
NXP Employee
NXP Employee

Hello Antonio,

Thanks for your comment!

I'm afraid there is no eCos example for S32DS currently available.

I'd not expect a serious problems porting your existing project from Sourcery to S32DS since they are both based on gcc.

Regarding MPC5668G/E - these are supported by CodeWarrior only. There is currently no plans to support it in S32DS.

Regards,

Stanislav

3,950 Views
antoniograu
Contributor II

Hello Stanislav,

thanks for your useful answer. I will try to port my current MPC5748G to S32DS and give some feedback.

Kind regards,
Antonio Grau

0 Kudos
Reply